After selection of your ZIP code, we designate the relevant staff to attend to you at once.
For the customer, the production must go on without problems and an energy supply system should accordingly function smoothly. That presupposes the effortless performance of all components and the cables used in them. igus® was the first company to develop a complete e-chain system®. chainflex® cables and e-chain® are supplied from one source and - according to application - offered with a system guarantee. The design principles that help to prevent machine downtimes all over the world have emerged and still develop from the know-how in cables that grew since 1989 and from a series of very laborious experiments.
Reliably closing doors secure subway operation of the VAG Nürnberg with chainflex® cables
15 years maintenance-free: How special cables keep a palletising system running - The energy supply system from igus covers 73 million double strokes without a cable failure and breaks all records in the process!
Gripper gymnastics in the chemist's shop - chainflex® cables in automated order picking systems
Play it safe - Flexible chainflex® cables provide additional safety for viastore storage and retrieval units
The gold vector award goes to Gildemeister Italiana S.p.A. from Italy with the multi-spindle lathe.
Flexible service providers in automation technology, who handle complex projects, need suppliers as flexible as igus GmbH.
It does not always have to be copper - MS Spaichingen uses chainflex® thermal compensation cable for innovative connection technology
Maintenance platform for WKA rotors, equipped with maintenance-free products from igus.
Permanent connection - Tried and tested: Insulation displacement connection technology (IDC) in movable cable systems from igus® & HARTING
chainflex® cables are not only suitable for applications with energy chains but also with roller guides.
Tested cable/connector combinations increase the safety of machines
The hybrid cables of the chainflex® product range are tried and tested and used in the new flexible IMAGIC flex drilling systems.
This robot applies various materials to a floor: Special demands are made on the cables of the “Floor Master Robot”
A central task in the plant for iron alloys is performed by the conveyor belts which transport the raw material to the melt reduction furnaces.
An industrial camera monitors a robot which takes over the insertion of seals in the automotive industry.
Special, high tensile strength bus cables for chip card readers in a lift system.
Moving cables in high-speed use - igus energy chain systems in Hekuma plants
The combination of chainflex cables and MFP8 RJ45 plug connectors offers outstanding transmission characteristics even after millions of cycles.
Cables for 400 million strokes in ultra-fast pick-and-place movements.
Measuring system cable also transmits signals safely over large distances and thus ensures high machine availability.
Lower weight and space requirements than alternative solutions for conveying coal.
These applications test systems that will make driving cars safer.
The motors in this system need a large number of cables.
Quick tool changes permit continuous machining of metal bands on both sides.
No more malfunctions when dosing fluids with precision.
No more cork screws and cable failures when transporting roof shingles.
An asphalting system prototype that uses a pick&place portal to distribute the material from each batch.
Due to the high robustness and stability, in a wastewater treatment plant near Saale, the decision was made for an E2/000 e-chain®.
For protection against outdoor influences the connection cables of the solar cell were mounted in an E2 micro energy chain.
17 million cycles per year – chainflex® cables for PCB assembly machine.
chainflex® control cables significantly reduce the failure rate of the machine in the concrete factory.
Temperature-resistant chainflex® cables in an LED screen.
Energy chain system instead of cable drum - Smooth operation at the sewage treatment plant since 2000
Control cables for extremely small bend radii in the passenger compartment doors in public transport vehicles.
300,000 double strokes a month impose rigorous requirements on the control cable.
Heat, abrasive dirt, high atmospheric moisture: These are only some of the ambient conditions in a composting plant.
Cables with high bending strength increase machine availability in the furniture industry.
Thanks to the construction with e-chains® in the thermal spas in Bad Wörishofen, about 100 meters of cable could be saved and the weight of the roof was reduced.
The igus® preassembled energy chains create a lasting, low-wear connection to the tools.
Top condition even after 9 years - Preassembled energy supply systems for precision machines working under tough environmental conditions
The demands on the facility are very high. All parts of the elevator are permanently exposed to wind and weather, and additional centrifugal forces act upon the parts by the 180° rotation.
Crane travels up to 500 m with energy chain systems and cables from igus®.
Tests showed that the Micro flizz® can also be operated in tough test conditions in the cold chamber at -40°C and today it is standard equipment of the new generation high speed lifting doors.
Extreme stressing from tile dus in the building material industry.
The applied material repels chips with temperatures up to 850° C without leaving a trace.
Rigorous requirements imposed on the energy supply: Cycle times and narrow bend radii are a considerable strain on energy supply and lines.
Here an energy supply system was developed from standard parts, whose piggyback system at last allocates a
defined place for the large volume suction hoses.
For this milling machine only energy chains were considered that could satisfy the complex requirements occasioned by the high feed rates and the bend radii.
With readychain energy supply systems, the customer receives all components from a single source and everything is ready to install.
In crane construction, energy supply systems frequently prove their technical and economic strengths. Flexibility, variability and a space-saving installation are only some of the most important criteria.
Preassembled energy supply systems come into operation here. They provide the edge to cut down the cost of the process.
Energy supply systems for shipyard cranes successfully in operation since six years.
441 m travel: Reduction of tensile forces by about 75%.
Since the ship loader started operations in 2000, no troubles, either mechanical or in the cables, have occurred in the energy chain area.
Higher variability at lower costs - Multidimensional energy supply systems raise the performance of robots.
Robotic handling system for circuit boards. Flexible energy supply system in use in clean room technology.
A plastic chain makes any kind of maintenance on the open sea obsolete; a conventional metal chain would not be adequate for the combination of technical, climatic and mechanical requirements.
A very high acceleration provided an enormouschallenge for the design engineers of this robot.
Previously used cables have been replaced by flexible CF9 TPE control cables, which have a significantly longer service life.
The used igus® products prove themselves till today and drastically reduce the maintenance input.
In the case of this adhesive resin system, a lifting platform moves upwardto a height three or four times a day to empty barrels with a volume ofapprox. 200 litres.
Series CF27.D servo cables in underwater applications.
Flexible chainflex® CF9 control cables and various hoses in zig-zag application.
Highly flexible chainflex® control cables in TV production.
Operational safety in low-floor vehicles thanks to chainflex® control cable for extremely small bend radii.
The technical demands on energy supply systems in machinery and plant construction require cables that work reliably.
Energy supply systems demonstrate their reliability even in particularly aggressive environmental conditions in special-purpose machinery construction.
The chainflex® bus cables are used for their robustness and signal quality.
Energy supply systems and cables for the highest demands in linear drive technology.
Conversion of a go-cart with combustion engine into an electric go-cart with maximum driving pleasure.
The unusual design for a recumbent bicycle has got what it takes: cordless screwdrivers are used here to drive it.
To the quarter finals of EUROBOT 2009 with the robot "elephant".
Outdoor cranes must withstand harsh weather conditions. Indoor cranes also work under alternating moisture influences with simultaneous extremely high temperatures.
This robot checks ventilation shafts before and after cleaning. Energy supply is via a cable
Robust chainflex® cable CF 9 also withstands adverse weather conditions.
The winner of this year’s golden vector is also the longest travel ever to be realised with plastic energy chains in the world.
Maintenance free with cables and multi-dimensional energy chains.